3.2.21 Digital Filter

Below is a list of API functions output by the Code Generator for digital filter use.

Table 3.21

API Functions: [Digital filter]

API Function Name

Function

R_DFE_Create

Performs initialization necessary to control the digital filter functions.

R_DFE_Create_UserInit

Performs user-defined initialization relating to the digital filter functions.

r_dfe_error_interrupt

Performs processing in response to the DFE error interrupt.

R_DFE_Set_SoftwareData

Sets the data to be processed.in a target filter.

R_DFE_Generate_SoftwareTrigger

Generates the software trigger.

R_DFE_Channelm_Create

Performs initialization necessary to control the digital filter channel functions.

R_DFE_Channelm_Create_UserInit

Performs user-defined initialization relating to the digital filter channel functions.

r_dfe_channelm_interrupt

Performs processing in response to the DFE channel interrupt.

r_dfe_channelm_callback_output_data

Performs processing in response to the output data interrupt.

r_dfe_channelm_callback_condition_match

Performs processing in response to the condition match interrupt.

R_DFE_Channelm_Enable

Enables the DFE channel.

R_DFE_Channelm_Disable

Disables the DFE channel.

R_DFE_Channelm_GetResult

Reads the results of DFE processing calculation.