Below is a list of API functions output by the Code Generator for 16-bit wakeup timer (WUTM) use.
Table 3.18 API Functions: [16-bit Wakeup Timer]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 16-bit wakeup timer. | |
|
Performs user-defined initialization relating to the 16-bit wakeup timer. | |
|
Performs processing in response to the timer interrupt. | |
|
Starts the count for 16-bit wakeup timer. | |
|
Ends the count for 16-bit wakeup timer. | |
|
Halts the clock supplied to the 16-bit wakeup timer. |