Below is a list of API functions output by the Code Generator for serial array unit 4 (DALI/UART4) use.
Table 3.32 API Functions: [Serial Array Unit 4]
|
API Function Name |
Function |
|
Performs initialization necessary to control the serial array unit 4 (DALI/ UART4). | |
|
Performs processing in response to the DALI transmission end interrupt INTSTDLn. | |
|
Performs processing in response to the DALI reception end interrupt INTSRDLn. | |
|
Performs processing in response to the DALI reception error interrupt INTSREDLn. | |
|
Sets DALI communication to standby mode. | |
|
Ends DALI communication. | |
|
Starts DALI data transmission. | |
|
Starts DALI data reception. | |
|
Performs processing in response to the DALI transmission end interrupt INTSTDLn. | |
|
Performs processing in response to the DALI reception end interrupt INTSRDLn. | |
|
Performs processing in response to the DALI reception error interrupt INTSREDLn. | |
|
Performs processing in response to detection of overrun error. |