Below is a list of API functions output by the Code Generator for timer RD use.
Table 3.7 API Functions: [Timer RD]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 16-bit timer RDn. | |
|
Performs user-defined initialization relating to the 16-bit timer RDn. | |
|
Performs processing in response to the timer interrupt. | |
|
Starts the count for 16-bit timer RDn. | |
|
Ends the count for 16-bit timer RDn. | |
|
Halts the clock supplied to the 16-bit timer RDn. | |
|
Starts the pulse output forced cutoff for 16-bit timer RDn, | |
|
Ends the pulse output forced cutoff for 16-bit timer RDn. | |
|
Reads the pulse width of the 16-bit timer RDn. | |
|
Performs initialization necessary to control the 16-bit timer RDn. | |
|
Performs user-defined initialization relating to the 16-bit timer RDn. | |
|
Performs processing in response to the timer interrupt. | |
|
Starts the count for 16-bit timer RDn. | |
|
Ends the count for 16-bit timer RDn. | |
|
Halts the clock supplied to the 16-bit timer RDn. | |
|
Starts the pulse output forced cutoff for 16-bit timer RDn, | |
|
Ends the pulse output forced cutoff for 16-bit timer RDn. | |
|
Reads the pulse width of the 16-bit timer RDn. | |
|
Halts the clock supplied to the 16-bit timer RD. |