Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the arbitration-lost detection, NACK detection, and timeout detection.
Remark This API function is called as the r_riicn_error_interrupt callback routine.
[Syntax]
#include "r_cg_macrodriver.h"
static void r_riicn_callback_receiveerror ( MD_STATUS status );
Remark n is the channel number.
[Argument(s)]
| 
 I/O  | 
 Argument  | 
 Description  | 
| 
 I  | 
 MD_STATUS status;  | 
 Source of the transfer errors and event generation interrupts MD_ERROR1 : Arbitration-lost detection MD_ERROR2 : Timeout detection MD_ERROR3 : NACK detection  | 
[Return value]
None.