R_RIICn_Master_Send

Starts RIIC master transmission.

Remark 1. This API function handles RIIC master transmission to the slave device at the address specified by the argument adr and the R/W#bit. RIIC master transmission in byte units is repeated the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf.

Remark 2. This API function internally calls R_RIICn_StartCondition to handle processing to start RIIC master transmission.

Remark 3. When performing a RIIC master transmission, R_RIICn_Start must be called before this API function is called.

[Syntax]

#include "r_cg_macrodriver.h"

MD_STATUS R_RIICn_Master_Send ( uint16_t adr, uint8_t * const tx_buf, uint16_t tx_num );

Remark n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

uint16_t adr;

Slave address

I

uint8_t * const tx_buf;

Pointer to a buffer storing the transmission data

I

uint16_t tx_num;

Total amount of data to send

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR1

Bus busy

MD_ERROR2

Invalid argument adr specification