r_riicn_transmitend_interrupt

Performs processing in response to the transmit end interrupts (TEI).

Remark This API function is called to run interrupt processing for the transmit end interrupts (TEI).

[Syntax]

static void r_riicn_transmitend_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.