Issues the start condition and causes a transfer error and an event generation interrupt (EEI).
Remark 1. This API function is called as the internal function of R_RIICn_Master_Send and R_RIICn_Master_Receive.
Remark 2. r_riicn_error_interrupt is called in response to calling of this API function.
[Syntax]
void R_RIICn_StartCondition ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.