2.5 Output Source Code

Output the source code (device driver program) by pressing the button on the Peripheral Functions panel.

The destination folder for the source code is specified by clicking [Code Generator Setting] tab >> [Generate File Mode] >> [Output folder] in the Property panel.

Figure 2.5

Output Source Code

 

Remark

In order to both output source files and add them to the project (display the corresponding source file names in the Project Tree panel) when you click the button, you must open the Property panel, and under [Code Generator Setting] tab >> [Generate File Mode] >> [Register files], specify "Register the generated files to the project".

Figure 2.6

Configure Whether to Register