[RI850V4] tab

Outline

This tab shows the detailed information on RI850V4 to be used categorized by the following.

- Version Information

This tab can be opened as follows:

- On the Project Tree panel, select a component such as the Realtime OS node or the system configuration file, and then select the [View] menu -> Property] or select [Property] from the context menu.

Note When the Property panel is already open, selecting a component such as the Realtime OS node or the system configuration file on the Project Tree panel displays the detailed information regarding the selected component.

Display image



Explanation of each area

1 ) [Version Information]

The detailed information on the version of the RI850V4 are displayed.

Kernel version

Display the version of RI850V4 to be used.

Default

The latest version of the installed RI850V4 package

How to change

Changes not allowed

Install folder

Display the folder in which RI850V4 to be used is installed with the absolute path.

Default

The folder in which RI850V4 to be used is installed

How to change

Changes not allowed

Register mode

Display the register mode set in the project.

Display the same value as the value of the [Select register mode] property of the build tool.

Default

The register mode selected in the property of the build tool

How to change

Changes not allowed