Renesas Electronics
sns_ctx Outline Reference contexts. C format BOOL sns_ctx (void); Parameter(s) None. Explanation This service call acquires the context type of the processing program that issued this service call (non-task context or task context). When this service call is terminated normally, the acquired context type (TRUE: non-task context, FALSE: task context) is returned. Return value Macro Value Description TRUE 1 Normal completion (non-task contexts). FALSE 0 Normal completion (task contexts).
BOOL sns_ctx (void);