sns_dpn

Outline

Reference dispatch pending state.

C format

 BOOL    sns_dpn (void);
Parameter(s)

None.

Explanation

This service call acquires the system status type when this service call is issued (whether in dispatch pending state or not).

When this service call is terminated normally, the acquired system state type (TRUE: dispatch pending state, FALSE: dispatch not-pending state) is returned.

Return value

Macro

Value

Description

TRUE

1

Normal completion. (dispatch pending state)

FALSE

0

Normal completion. (any other states)