Renesas Electronics
sns_loc Outline Reference CPU state. C format BOOL sns_loc (void); Parameter(s) None. Explanation This service call acquires the system status type when this service call is issued (CPU locked state or CPU unlocked state). When this service call is terminated normally, the acquired system state type (TRUE: CPU locked state, FALSE: CPU unlocked state) is returned. Return value Macro Value Description TRUE 1 Normal completion (CPU locked state). FALSE 0 Normal completion (CPU unlocked state).
BOOL sns_loc (void);