-
unl_cpu
iunl_cpu
-
ER unl_cpu (void);
ER iunl_cpu (void);
These service calls change the system status from the CPU locked state to the CPU unlocked state.
As a result, "EI level maskable interrupt acceptance" and "service call issue" restricted (prohibited) through issue of loc_cpu or iloc_cpu are enabled.
If an EI level maskable interrupt is created during the interval from when either
loc_cpu or
iloc_cpu is issued until this service call is issued, the RI850V4 delays transition to the relevant interrupt processing (interrupt handler) until this service call is issued.
Note 1 This service call does not perform queuing of cancellation requests. If the system is in the CPU unlocked state, therefore, no processing is performed but it is not handled as an error.
Note 2 This service call manipulates PM
n bits in the priority mask register (PMR) to disable acceptance of EI level maskable interrupts.
The PM
n bits to be manipulated correspond to the interrupt priority range defined as the
Maximum interrupt priority: maxintpri during configuration.
This service call does not manipulate the ID bit in the program status word (PSW).
Note 3 This service call does not cancel the dispatch disabled state that was set by issuing
dis_dsp. If the system status before the CPU locked state is entered was the dispatch disabled state, the system status becomes the dispatch disabled state after this service call is issued.
Note 4 If a service call other than
loc_cpu,
iloc_cpu and sns_
xxx is issued from when
loc_cpu or
iloc_cpu is issued until this service call is issued, the RI850V4 returns E_CTX.