Renesas Electronics
Below is a list of API functions output by the Code Generator for clock serial interface H use.
Table 3.8
API Functions: [Clock serial interface H]
API Function Name
Function
R_CSIHm_Create
Performs initialization necessary to control the clock serial interface H functions.
R_CSIHm_Create_UserInit
Performs user-defined initialization relating to the clock serial interface H functions.
r_csihm_interrupt_receive
Performs processing in response to the CSIH reception interrupt.
r_csihm_interrupt_error
Performs processing in response to the CSIH error interrupt.
r_csihm_interrupt_send
Performs processing in response to the CSIH communication interrupt.
r_csihm_interrupt_jobend
Performs processing in response to the CSIH job end interrupt.
r_csihm_callback_receiveend
r_csihm_callback_sendend
r_csihm_callback_error
R_CSIHm_Start
Sets CSIH communication to standby mode.
R_CSIHm_Stop
Ends CSIH communication.
R_CSIHm_Master_Send
Start CSIH data transmission by master mode.
R_CSIHm_Master_Receive
Start CSIH data reception by master mode.
R_CSIHm_Slave_Send
Start CSIH data transmission by slave mode.
R_CSIHm_Slave_Receive
Start CSIH data reception by slave mode.
R_CSIHm_Extended_Data_Master_Send
Start CSIH extended data transmission by master mode.
R_CSIHm_Extended_Data_Master_Receive
Start CSIH extended data reception by master mode.
R_CSIHm_Extended_Slave_Send
Start CSIH extended data transmission by slave mode.
R_CSIHm_Extended_Data_Slave_Receive
Start CSIH extended data reception by slave mode.