Renesas Electronics
Below is a list of API functions output by the Code Generator for Interrupt use.
Table 3.4
API Functions: [Interrupt]
API Function Name
Function
R_INTC_Create
Performs initialization necessary to control the interrupt functions.
R_INTC_Create_UserInit
Performs user-defined initialization relating to the interrupt functions.
R_IRQn_Start
Enables the IRQn interrupts.
R_IRQn_Stop
Disables the IRQn interrupts.
R_SINTn_Start
Enables the software interrupts (SINTn).
R_SINTn_Stop
Disables the software interrupts (SINTn).
R_SINTn_TriggerOn
Software interrupt registers increments the value of a counter.
R_INTPn_Start
Enables the INTPn interrupts.
R_INTPn_Stop
Disables the INTPn interrupts.
r_nmi_interrupt
Performs processing in response to the NMI interrupt.
r_irqn_interrupt
Performs processing in response to the IRQn interrupt.
r_sintn_interrupt
Performs processing in response to the SINTn interrupt.
r_intpn_interrupt
Performs processing in response to the INTPn interrupt.