3.2.15 Timer Array Unit D

Below is a list of API functions output by the Code Generator for timer array unit D use.

Table 3.15

API Functions: [Timer array unit D]

API Function Name

Function

R_TAUDn_Create

Performs initialization necessary to control the timer array unit Dn.

R_TAUDn_Create_UserInit

Performs user-defined initialization relating to the timer array unit Dn.

r_taudn_channelm_interrupt

Performs processing in response to the timer interrupt.

R_TAUDn_Channelm_Start

Starts the count for channel m.

R_TAUDn_Channelm_Stop

Ends the count for channel m.

R_TAUDn_Channelm_Get_PulseWidth

Reads the input pulse width of the timer.