3.2.14 Timer Array Unit B

Below is a list of API functions output by the Code Generator for timer array unit B use.

Table 3.14

API Functions: [Timer array unit B]

API Function Name

Function

R_TAUBn_Create

Performs initialization necessary to control the timer array unit Bn.

R_TAUBn_Create_UserInit

Performs user-defined initialization relating to the timer array unit Bn.

r_taubn_channelm_interrupt

Performs processing in response to the timer interrupt.

R_TAUBn_Channelm_Start

Starts the count for channel m.

R_TAUBn_Channelm_Stop

Ends the count for channel m.

R_TAUBn_Channelm_Get_PulseWidth

Reads the input pulse width of the timer.