This dialog box is used to display and modify detailed information on an access-related event selected in the Events panel.
Note that the access-related events refer to the following events in the Events panel.
 
 
 
This section describes the following.
| On the Events panel, move the caret to any one of the following events, and then select [Edit Condition...] from the context menu. | 
Specify the address condition.
| Specifies the address with [Address]. | ||||
| Specifies the range with [Start address] and [End address]. | ||||
| This item appears only when [Specified address (==)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition]. | ||||
| This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition]. | ||||
| This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition]. | ||||
| Specify the value of address mask. This item appears only when [Use the address mask] is set to [Yes]. | ||||
| Specifies the data with [Compare data]. | ||||
| Specifies the range with [Lower data] and [Upper data]. | ||||
| This item appears only when [Specified value (==)], [Any other value (!=)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition]. | ||||
| Specify the lower data for the range in [Compare condition]. This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition]. | ||||
| Specify the upper data for the range in [Compare condition]. This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition]. | ||||
| Specify the value of data mask. This item appears only when [Use the data mask] is set to [Yes]. | ||||
Specify the pass count condition.
| The relevant event occurs when the event condition is met as many times as the specified pass count. | ||||
This area displays a simple description of the item selected in the Event conditions setting area.
| Displays all categories in the Event conditions setting area. | ||
| Hides categories in the Event conditions setting area and rearranges only setting items in the ascending order | ||