|
Current Consumption Measurement Condition Setting dialog box [E2] |
This dialog box is used to set measurement conditions in the Measuring Current Consumption panel [E2][Simulator].
This section describes the following.
On the Measuring Current Consumption panel [E2][Simulator], click the |
Select the operation of the debugger after the recording memory of the emulator becomes full during the measurement of current consumption from the following drop-down list.
Select the sampling time during the measurement of current consumption.
The following sampling times can be selected.
1us, 2us, 5us, 10us, 20us, 50us, 100us, 200us, 500us, 1ms
Make settings regarding conditions for writing to the recording memory of the emulator.
Select the type of condition for writing to the recording memory of the emulator from the following drop-down list.
When "During detecting an external trigger input" is selected for [Condition], select "ch0" or "ch1" as the external trigger input channel from the extended interface of the E2 emulator that is to be detected.
When "During detecting an external trigger input" is selected for [Condition], select "High" or "Low" as the level of the external trigger input signal to be detected.
When "During monitor points" is selected for [Condition], select the two target monitoring points.
Monitoring points that have currently been specified for the project are displayed in a drop-down list.
The measured data will only be recorded from the time the monitoring point set in the left side has been detected until detection of the monitoring point set on the right side.
|
Reflects the settings of the measurement conditions that were made in this dialog box to the Measuring Current Consumption panel [E2][Simulator]. |
|
button on the toolbar.