| 
 Memory Mapping dialog box 
 | 
This dialog box is used to display the state of the memory mapping.
Figure A.19  | Memory Mapping Dialog Box  | 
 
 
This section describes the following. 
[How to open]
Caution  | This dialog box cannot be opened during execution of a program.   | 
 
[Description of each area]
(1)  | Added memory mapping specification area  | 
 
This area is always invalid. 
(2)  | [Memory mapped list] area  | 
 
Information about the microcontroller's internal memory mapping is displayed. 
This area cannot be edited.
| 
 
Memory type 
 | 
 
Displays the memory types.  
 | 
| 
 
Address range 
 | 
 
Displays the address range as <Start address> - <End address>.  
Display is fixed as "0x"-prefixed hexadecimal numbers.  
 | 
| 
 
Size 
 | 
 
Displays size as a decimal number (unit: bytes/KbytesNote).  
 | 
| 
 
Access width 
 | 
 
Displays the access width (unit: bits).  
 | 
 
Note  | Only in the case of multiple of 1024, displays in kilobyte units.  | 
 
| 
 | 
 | 
| 
 
Remove 
 | 
 
This button is always invalid. 
 | 
 
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Closes this dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box.  
 |