With regard to the analysis information that was saved by pressing the button located on the Toolbar on the Realtime OS Task Analyzer panel, the user can restore it to the Child-panel display area on the Realtime OS Task Analyzer panel by selecting either [Open trace data...] or [Task analyzer trace data name] from the drop-down list located on the Toolbar on the Realtime OS Task Analyzer panel.
When selecting the [Open trace data....] on the drop-down list, select/specify the folder and the file in which the task analyzer trace data is stored, in the Open dialog box which is opened when the menu is selected.