Everything
2.4 Open Analysis Result Panel

To view analysis information, such as the state of processing program execution, the state of real-time OS resource usage, and the CPU usage status, open the Analysis Result panel.

The Analysis Result panel can be opened by pressing the button which is located on the Toolbar on the Realtime OS Task Analyzer panel.

Figure 2.2

Analysis Result Panel