Everything

R_TMRDn_Set_PowerOff

Halts the clock supplied to the 16-bit timer RDn.

Remark         Calling this API function changes the 16-bit timer RDn to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

 

[Syntax]

void   R_TMRDn_Set_PowerOff ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.