Ends the pulse output forced cutoff for 16-bit timer RDn.
Remark This API function can only be called when the 16-bit timer RDn is the count to stopped (the TSTART bit in the timer RD start register (TRDSTR) is 0).
[Syntax]
void R_TMR_RDn_ForcedOutput_Stop ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.