Everything

R_TMR_RDn_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RDn.

Remark         This API function is called as the R_TMR_RDn_Create callback routine.

 

[Syntax]

void       R_TMR_RDn_Create_UserInit ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.