Everything

Timer RD

Below is a list of API functions output by the Code Generator for timer RD use.

 

Table 3.7   API Functions: [Timer RD]

API Function Name

Function

R_TMR_RDn_Create

Performs initialization necessary to control the 16-bit timer RDn.

R_TMR_RDn_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RDn.

r_tmr_rdn_interrupt

Performs processing in response to the timer interrupt.

R_TMR_RDn_Start

Starts the count for 16-bit timer RDn.

R_TMR_RDn_Stop

Ends the count for 16-bit timer RDn.

R_TMR_RDn_Set_PowerOff

Halts the clock supplied to the 16-bit timer RDn.

R_TMR_RDn_ForcedOutput_Start

Starts the pulse output forced cutoff for 16-bit timer RDn,

R_TMR_RDn_ForcedOutput_Stop

Ends the pulse output forced cutoff for 16-bit timer RDn.

R_TMR_RDn_Get_PulseWidth

Reads the pulse width of the 16-bit timer RDn.

R_TMRDn_Create

Performs initialization necessary to control the 16-bit timer RDn.

R_TMRDn_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RDn.

r_tmrdn_interrupt

Performs processing in response to the timer interrupt.

R_TMRDn_Start

Starts the count for 16-bit timer RDn.

R_TMRDn_Stop

Ends the count for 16-bit timer RDn.

R_TMRDn_Set_PowerOff

Halts the clock supplied to the 16-bit timer RDn.

R_TMRDn_ForcedOutput_Start

Starts the pulse output forced cutoff for 16-bit timer RDn,

R_TMRDn_ForcedOutput_Stop

Ends the pulse output forced cutoff for 16-bit timer RDn.

R_TMRDn_Get_PulseWidth

Reads the pulse width of the 16-bit timer RDn.

R_TMRD_Set_PowerOff

Halts the clock supplied to the 16-bit timer RD.