R_TMR_KBm_ForcedOutput_mn_Start
Enables input of the trigger signal
used for the forced output stop function.
[Syntax]
void
R_TMR_KBm_ForcedOurput_mn_Start ( void );
Remark
m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return
value]
None.