16-bit timer KB
Below is a list of API functions output by the Code Generator for 16-bit timer KB use.
Table 3.10 API Functions: [16-bit Timers KB]
API Function Name |
Function |
Performs initialization necessary to control the 16-bit timer KB. | |
Performs user-defined initialization relating to the 16-bit timer KB. | |
Performs processing in response to the timer interrupt. | |
Starts the count for 16-bit timer KB. | |
Ends the count for 16-bit timer KB. | |
Halts the clock supplied to the 16-bit timer KB. | |
Enables input of the trigger signal used for the forced output stop function. | |
Disables input of the trigger signal used for the forced output stop function. | |
Enables batch overwriting of the compare register. | |
Enables input of the trigger signal used for the forced output stop function. | |
Disables input of the trigger signal used for the forced output stop function. | |
Reset the 16-bit timer KB. |