Halts the clock supplied to the 16-bit timer KB.
Remark
Calling this API function changes the
16-bit timer KB to reset status.
For this reason, writes to the
control registers after this API function is called are ignored.
[Syntax]
void R_TMR_KBm_Set_PowerOff ( void );
[Argument(s)]
None.
[Return value]
None.