Everything

R_TMR_KBmn_ForcedOutput_Start

Enables input of the trigger signal used for the forced output stop function.

 

[Syntax]

void   R_TMR_KBmn_ForcedOurput_Start ( void );

Remark         m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.