Everything

r_uartfn_callback_error

Performs processing in response to the LIN-UART reception status interrupt INTLS.

Remark         This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS.

 

[Syntax]

static void   r_uartfn_callback_error ( uint8_t err_type );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

O

uint8_t err_type;

Trigger for LIN-UART reception status interrupt

  00000xx1B:         Overrun error

  00000x1xB:         Parity error

  000001xxB:         Framing error

 

[Return value]

None.