Everything
Everything
top
RL78 API Reference
API FUNCITONS
Function Reference
Asynchronous serial interface LIN-UART
Usage example
Usage example
Please refer to ‘
Usage example in 3.2.30 Serial Array Unit
’ when using this module as UART.
Differences Information
Previous Topic
r_uartfn_callback_idmatch
Next Topic
Serial interface IICA
Table of Contents
R_UARTFn_Create
R_UARTFn_Create_UserInit
r_uartfn_interrupt_send
r_uartfn_interrupt_receive
r_uartfn_interrupt_error
R_UARTFn_Start
R_UARTFn_Stop
R_UARTFn_Set_PowerOff
R_UARTFn_Send
R_UARTFn_Receive
R_UARTFn_Set_DataComparisonOn
R_UARTFn_Set_DataComparisonOff
r_uartfn_callback_sendend
r_uartfn_callback_receiveend
r_uartfn_callback_error
r_uartfn_callback_softwareoverrun
r_uartfn_callback_expbitdetect
r_uartfn_callback_idmatch
Usage example