Asynchronous serial interface LIN-UART
Below is a list of API functions output by the Code Generator for asynchronous serial interface LIN-UART (UARTF) use.
Table 3.33 API Functions: [Asynchronous Serial Interface LIN-UART]
API Function Name |
Function |
Performs initialization necessary to control the asynchronous serial interface LIN-UART (UARTF). | |
Performs user-defined initialization related to the asynchronous serial interface LIN-UART (UARTF). | |
Performs processing in response to the LIN-UART transmission end interrupt INTLT. | |
Performs processing in response to the LIN-UART reception end interrupt INTLR. | |
Performs processing in response to the LIN-UART reception status interrupt INTLS. | |
Sets LIN communication to standby mode. | |
Ends LIN communication. | |
Halts the clock supplied to the asynchronous serial interface LIN-UART (UARTF). | |
Starts UARTF data transmission. | |
Starts UARTF data reception. | |
Starts the data comparison. | |
Ends the data comparison. | |
Performs processing in response to the LIN-UART transmission end interrupt INTLT. | |
Performs processing in response to the LIN-UART reception end interrupt INTLR. | |
Performs processing in response to the LIN-UART reception status interrupt INTLS. | |
Performs processing in response to detection of overrun error. | |
Performs processing in response to detection of expansion bit. | |
Performs processing in response to match of ID parity. |