Performs processing in response to match ID parity.
Remark This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS (performed when ID parity has been matched).
[Syntax]
static void r_uartfn_callback_idmatch ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.