Everything

r_uartmgn_callback_receiveend

Performs processing in response to the UARTMG reception completion interrupt INTSRMGn.

Remark         This API function is called as the callback routine of interrupt process r_uartmgn_interrupt_receive corresponding to the UARTMG reception completion interrupt INTSRMGn (performed when number of received data specified by R_UARTMGn_Receive argument rx_num has been completed).

 

[Syntax]

static void   r_uartmgn_callback_receiveend ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.