Everything

R_UARTMGn_Send

Starts UARTMG data transmission.

Remarks 1.    This API function repeats the byte-level UART transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.

Remarks 2.    When performing a UART transmission, R_UARTMGn_Start must be called before this API function is called.

 

[Syntax]

#include       “r_cg_macrodriver.h”

MD_STATUS   R_UARTMGn_Send ( uint8_t * const tx_buf, uint16_t tx_num );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

I

uint8_t * const tx_buf;

Pointer to a buffer storing the transmission data

I

uint16_t tx_num;

Total amount of data to send

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification