Everything

r_uartmgn_callback_softwareoverrun

Performs processing in response to detection of overrun error.

Remark         This API function is called as the callback routine of interrupt process r_uartmgn_interrupt_receive corresponding to the UARTMG reception end interrupt INTSRMGn (process performed when the amount of data received is greater than the argument rx_num specified for R_UARTMGn_Receive).

 

[Syntax]

#include    “r_cg_macrodriver.h”

static void   r_uartmgn_callback_softwareoverrun ( uint16_t rx_data );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

I

uint16_t rx_data;

Receive data (greater than the argument rx_num specified for R_UARTMGn_Receive)

 

[Return value]

None.