Everything

r_uartmgn_callback_sendend

Performs processing in response to the UARTMG transmission complition interrupt INTSTMGn.

Remark         This API function is called as the callback routine of interrupt process r_uartmgn_interrupt_send corresponding to the UARTMG transmission completion interrupt INTSTMGn (performed when number of transmission data specified by R_UARTMGn_Send argument tx_num has been completed).

 

[Syntax]

static void   r_uartmgfn_callback_sendend ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.