frsm_tsk
ifrsm_tsk
ER frsm_tsk (ID tskid);
ER ifrsm_tsk (ID tskid);
These service calls cancel all of the suspend requests issued for the task specified by parameter tskid (by setting the suspend request counter to 0x0). As a result, the target task moves from the SUSPENDED state to the READY state, or from the WAITING-SUSPENDED state to the WAITING state.
Note This service call does not perform queuing of cancellation requests. If the target task is in a state other than the SUSPENDED or WAITING-SUSPENDED state, "E_OBJ" is therefore returned.