Everything

sns_dsp

Outline
Reference dispatching state.
C format
 BOOL      sns_dsp (void);
Parameter(s)
None.
Explanation
This service call acquires the system status type when this service call is issued (dispatch disabled state or dispatch enabled state).
When this service call is terminated normally, the acquired system state type (TRUE: dispatch disabled state, FALSE: dispatch enabled state) is returned.
Return value
Macro
Value
Description
TRUE
1
Normal completion (dispatching disabled state).
FALSE
0
Normal completion (dispatching enabled state).