Everything

sns_loc

Outline
Reference CPU state.
C format
 BOOL    sns_loc (void);
Parameter(s)
None.
Explanation
This service call acquires the system status type when this service call is issued (CPU locked state or CPU unlocked state).
When this service call is terminated normally, the acquired system state type (TRUE: CPU locked state, FALSE: CPU unlocked state) is returned.
Return value
Macro
Value
Description
TRUE
1
Normal completion (CPU locked state).
FALSE
0
Normal completion (CPU unlocked state).