The adf, sbf, sasf, and setf instructions of the device should be specified in the following formats. |
Code that can be specified in cond and the result of assembly are shown in "Table 5.27 setfcond Instruction", using the setf instruction as an example. |