- | The divh instructions of the device should be specified in the following formats. |
- | In asrh, the following formats can also be used in addition to the above. |
- | If the instruction is executed in syntax "divh imm, reg2", and the following expression is specified for imm, the assembler executes instruction expansion to generate multiple machine instructions. |
(a) | Absolute expression having a value of other than 0 within the range of -16 to +15 |
|
|
divh imm5, reg
|
mov imm5, r1
divh r1, reg
|
(b) | Absolute expression exceeding the range of -16 to +15, but within the range of -32,768 to +32,767 |
|
|
divh imm16, reg
|
movea imm16, r0, r1
divh r1, reg
|
(c) | Absolute expression having a value exceeding the range of -32,768 to +32,767 |
If all the lower 16 bits of the value of imm are 0
|
|
divh imm, reg
|
movhi HIGHW(imm), r0, r1
divh r1, reg
|
Else
|
|
divh imm, reg
|
mov imm, r1
divh r1, reg
|
(d) | Relative expression having !label or %label, or that having $label for a label having a definition in the sdata/sbss-attribute section |
|
|
divh !label, reg
|
movea !label, r0, r1
divh r1, reg
|
divh %label, reg
|
movea %label, r0, r1
divh r1, reg
|
divh $label, reg
|
movea $label, r0, r1
divh r1, reg
|
(e) | Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section |
|
|
divh #label, reg
|
mov #label, r1
divh r1, reg
|
divh label, reg
|
mov label, r1
divh r1, reg
|
divh $label, reg
|
mov $label, r1
divh r1, reg
|
- | If the instruction is executed in syntax "divh imm, reg2, reg3", and the following expression is specified for imm, the assembler executes instruction expansion to generate one or more machine instructions. |
|
|
divh 0, reg2, reg3
|
divh r0, reg2, reg3
|
(b) | Absolute expression having a value of other than 0 within the range of -16 to +15 |
|
|
divh imm5, reg2, reg3
|
mov imm5, r1
divh r1, reg2, reg3
|
(c) | Absolute expression exceeding the range of -16 to +15, but within the range of -32,768 to +32,767 |
|
|
divh imm16, reg2, reg3
|
movea imm16, r0, r1
divh r1, reg2, reg3
|
(d) | Absolute expression having a value exceeding the range of -32,768 to +32,767 |
If all the lower 16 bits of the value of imm are 0
|
|
divh imm, reg2, reg3
|
movhi HIGHW(imm), r0, r1
divh r1, reg2, reg3
|
Else
|
|
divh imm, reg2, reg3
|
mov imm, r1
divh r1, reg2, reg3
|
(e) | Relative expression having !label or %label, or that having $label for a label having a definition in the sdata/sbss-attribute section |
|
|
divh !label, reg2, reg3
|
movea !label, r0, r1
divh r1, reg2, reg3
|
divh %label, reg2, reg3
|
movea %label, r0, r1
divh r1, reg2, reg3
|
divh $label, reg2, reg3
|
movea $label, r0, r1
divh r1, reg2, reg3
|
(f) | Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section |
|
|
divh #label, reg2, reg3
|
mov #label, r1
divh r1, reg2, reg3
|
divh label, reg2, reg3
|
mov label, r1
divh r1, reg2, reg3
|
divh $label, reg2, reg3
|
mov $label, r1
divh r1, reg2, reg3
|