Everything

jarl


-

The jarl instructions of the device should be specified in the following formats.

-

JARL disp22, reg2

-

JARL disp32, reg1

-

JARL [reg1], reg3

 

-

In asrh, the following formats can also be used in addition to the above.

-

jarl22 disp, reg2

-

jarl32 disp, reg1

 

-

jarl instructions are interpreted as disp22 when the -Xasm_far_jump option is not specified, or disp32 when the -Xasm_far_jump option is specified.

-

jarl22 or jarl32 should be specified when output should be with a fixed disp width at all times. These instructions will not be affected by the -Xasm_far_jump option.