jmp
-
The jmp instructions of the device should be specified in the following formats.
JMP [reg1]
JMP disp32 [reg1]
In asrh, the following formats can also be used in addition to the above.
Format
Meaning
jmp disp32
jmp disp32[r0]
jmp32 [reg1]
jmp [reg1]
jmp32 disp32
jmp32 disp32[reg1]
jmp disp32[reg1]