This dialog box is used to set the memory mapping for each type of memory.
When the selected microcontroller supports multi-core, this property displays the memory mapping status regarding a core (PE) by switching selection between the target cores (see "2.9 Select a Core (PE)"). |


This section describes the following.
On the [Debug Tool Settings] tab of the Property panel, click the [...] button displayed by selecting one of the values of the [Memory mappings] property in the [Memory] category. |
Specify the information for a memory mapping newly added.
This area is always invalid except for in the simulator.
Select the memory type for the memory mapping to be added from the following drop-down list (The item selected by default differs depending on the debug tool to use).
This area is for testing and it can be accessed from the user program. It can be allocated to only space that overlaps with [Access prohibited]. |
Mapping attributes and their sizes that can be set are as follows:
Specify the start address and end address for the memory mapping to be added. Directly input a hexadecimal number into the text box for each.
In the case of the following settings, however, new memory mappings cannot be added (Clicking the [Add] button in this area causes an error message to be displayed).
If the specified address range duplicates the memory area other than [Access prohibited] when [Temporary] is selected as the memory type |
Adds the content specified in this area to memory mapping. The added memory mapping is displayed in the [Memory mapped list] area. The changes will not take effect until the [OK] button is clicked. |
Information about the memory mapping added in the Added memory mapping specification area and the microcontroller's internal memory mapping is displayed.
Displays the address range as <Start address> - <End address>. |
|
Displays size as a decimal number (unit: bytes/KbytesNote 3). |
|