You configure the basic settings of the debug tool for each one of the following categories.
(2) [Access Memory While Running]
You can configure the memory in this category.

Current memory mapping status is displayed for each type of memory area.
Select whether to perform a verify check when writing to the memory.
Select [Yes] to perform verification after download or when values are changed in the Memory panel/Watch panel (default).
You can configure the memory access while executing a program (the real-time display update function) in this category. See "2.9.1.4 Display/modify the memory contents during program execution" for details on the real-time display update function.

For a memory area not accessible during execution of a program (e.g. target memory area/SFR area), select whether to allow access to the area by temporary stopping the execution.
Select [Yes] to allow access (default: [No]).
Select whether to automatically update the contents in the Memory panel/Watch panel display during execution of a program.
Select [Yes] to update the display automatically (default).
The display contents of the Memory panel/Watch panel can be updated manually by clicking the |
This property appears only when the [Update display during the execution] property is set to [Yes].
Specify the interval in 100 ms unit to automatically update the contents in the Memory panel/Watch panel display during execution of a program.
Directly enter the Integer number between 100 and 65500 (rounding up the fractions less than 100ms) (default: [500]).
You can configure the setting of events while executing a program in this category.

Select whether to forcibly pause the execution for events that cannot be set while executing a program.
For details on the event types that are affected by this property, see "2.15.7.2 Event types that can be set and deleted during execution".
Select [Yes] to set events above while execution (default: [No]).
You can configure the break function.
See "2.8 Stop Programs (Break)" for details on the break function and this category configuration.
You can configure the fail-safe break function in this category.
See "2.8.6 Stop the program when an invalid execution is detected [IECUBE]" for details on the fail-safe break function and this category configuration.
You can configure the trace function in this category.
See "2.11 Collect Execution History of Programs" for details on the trace function and this category configuration.
You can configure the timer function in this category.
See "2.12 Measure Execution Time of Programs" for details on the timer function and this category configuration.
You can configure the coverage function in this category.
See "2.13 Measure Coverage [IECUBE][Simulator]" for details on the coverage function and this category configuration.
You can configure the input signal masking in this category.

With the properties shown below, select [Yes] to mask the signal from the drop-down list (default: [No]).
If [No] is selected with the [Connection with Target Board] property in the [Connect Setting] tab, these properties are fixed to [Yes] after connecting to the debug tool (changes not allowed). |
You can configure the control method of step execution.

Select whether to skip the target section.
Select [Yes] to skip the target section (default: [No]).
This property appears only when the [Skip target section] property is set to [Yes].
To specify a section, select the target property, then open the Specified Section dialog box by clicking the [...] button that appears on the right edge of the field.