Everything

2.1 Installing Real-time OS Package

This section describes how to install real-time OS package.
(1) Insert the CD-ROM into the drive.
The Preparing to Install page appears automatically.
After, please operate with displayed contents.
Figure 2-1. Preparing to Install Page
Remark If the page does not appear automatically, open "Install.hta" in the CD-ROM.