Everything

2.7 Start Resource Information Tool

When a program using the real-time OS feature is downloaded, the Realtime OS Resource Information panel is opened automatically.
From [View] menu, select [Realtime OS] >> [Resource Information]. The Realtime OS Resource Information panel opens.
Figure 2-4. [Resource Information] Item
Figure 2-5. Realtime OS Resource Information Panel
Remarks 1. When resource information tool has started, it isn't possible to start more resource information tool.
2. See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI850V4/RI850MP/RI78V4 Debug" for details.